Other Parts Discussed in Thread: AWR1443BOOST, MMWAVE-STUDIO, , UNIFLASH, AWR1443
Hello,
I have a problem with my DCA1000EVM and AWR1443BOOST boards. I want to use the MMWAVE-STUDIO to capture data from the DCA1000EVM. I have connected the boards with 60-pin socket, set the SOP at the AWR1443BOOST (SOP0 and SOP1 short-circuited, SOP2 open-circuited), and I have set up the switches on board the DCA1000EVM (Switch 1 and Switch 2) according to the User Guide.
Upon starting the MMWAVE-STUDIO, I reset the board, connect to the RS232 port, load the files, but then SPI connect button fails to respond and connect the SPI. Then, I push the "RF power up" button and I get this error message: ""[RadarAPI]: Error: ReadRegister failed with error -2".
I have followed religiously the instruction of the User Guide.
What do I need to do in order to solve my problem?
Thank you,
Stelios