In LM3644 datasheet, there are there modes(flash mode / torch mode / IR mode) than lm3644 can work on.
Activated by the enable register (0x01), setting mode M1, M0(bits(1:0)) to corresponding value.
As a matter of fact,
After pulling the HWEN and TORCH/TEMP pins HIGH, set reg0x01 to 0x02 or 0x82, read reg0x0a and reg0x0b, both of them are 0x00. Read reg0x05 is 0xBF. Read reg0x0b is 0x3F.
As the datasheet describe, it should work in Torch mode.
But the Led not lights are not on.
How to make it work in Torch mode?
BR
Carl