Hi,
When using Vcc of 5V can the two wire interface be 3.3V? In other words pins 6 and 7 are pulled up to 3.3V through a resistor. Is the logic voltage levels of SMBus(tm), also apply then to the two wire? Is there anything else I should consider for the use case I describe?
Thank you,
HSG