This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BOOSTXL-TUSS4440: DRV Rdy flag in GUI is always 0, with USB or Ext power does not matter. No echo.

Part Number: BOOSTXL-TUSS4440


Hi Team, 

Hoping for your assistance to confirm the functionality is still ok.

www.ti.com/.../slau822a.pdf

All echo traces are just flat noise. they have configured jumpers according to Table 1 to Standard and to USB ONLY. In both cases, VDRV Ready shown in Table 3 bit is zero. This means that the voltage does not reach the correct level with the internal converter or with an external power supply for the driver. This is likely why they are not receiving any echo.

Thank you

-Mark