Other Parts Discussed in Thread: SYSBIOS
I can't build DSS nor MSS projects, it gives me this error when I build DSS project.
I am using CCS v10.2 and following tools:
This error is same in Beamsteering example also
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I can't build DSS nor MSS projects, it gives me this error when I build DSS project.
I am using CCS v10.2 and following tools:
This error is same in Beamsteering example also
Hi,
The release notes mention that
C:\data-nobackup\2020\Automotive Toolbox\mmwave_automotive_toolbox_3_2_0__win\mmwave_automotive_toolbox_3_2_0\labs\lab0007_medium_range_radar\docs\MediumRangeRadar_Release_Notes.pdf mention that it is required to use mmWave SDK 3.5.0.4 (latest release)
Please use this SDK release and you should be able to build
thank you
Cesar
I have installed all required tool and also gives errors as following
**** Clean-only build of configuration Debug for project mrr_18xx_dss ****
"C:\\ti\\ccs1020\\ccs\\utils\\bin\\gmake" -k -j 8 clean -O
DEL /F "mrr_18xx_dss.hex" "configPkg\linker.cmd" "configPkg\compiler.opt" "mrr_18xx_dss.xe674"
DEL /F "Extended_Kalman_Filter_xyz.oe674" "clusteringDBscan.oe674" "dss_config_edma_util.oe674" "dss_data_path.oe674" "dss_main.oe674" "gen_twiddle_fft16x16.oe674" "gen_twiddle_fft32x32.oe674" "common\cfg.oe674"
DEL /F "Extended_Kalman_Filter_xyz.d" "clusteringDBscan.d" "dss_config_edma_util.d" "dss_data_path.d" "dss_main.d" "gen_twiddle_fft16x16.d" "gen_twiddle_fft32x32.d" "common\cfg.d"
RMDIR /S/Q "configPkg\"
Could Not Find E:\Workspace-3\mrr_18xx_dss\Debug\mrr_18xx_dss.hex
Could Not Find E:\Workspace-3\mrr_18xx_dss\Debug\mrr_18xx_dss.xe674
Could Not Find E:\Workspace-3\mrr_18xx_dss\Debug\Extended_Kalman_Filter_xyz.oe674
Could Not Find E:\Workspace-3\mrr_18xx_dss\Debug\common\cfg.oe674
Could Not Find E:\Workspace-3\mrr_18xx_dss\Debug\Extended_Kalman_Filter_xyz.d
Could Not Find E:\Workspace-3\mrr_18xx_dss\Debug\common\cfg.d
Finished clean
**** Build Finished ****
**** Build of configuration Debug for project mrr_18xx_dss ****
"C:\\ti\\ccs1020\\ccs\\utils\\bin\\gmake" -k -j 8 all -O
rm -f E:/Workspace-3/mrr_18xx_dss/mrr_18xx_dss.bin
Building file: "../dss_mrr.cfg"
Invoking: XDCtools
"C:/ti/xdctools_3_61_02_27_core/xs" --xdcpath="C:/ti/bios_6_83_00_18/packages;" xdc.tools.configuro -o configPkg -t ti.targets.elf.C674 -p ti.platforms.c6x:AWR16XX:false:600 -r release -c "C:/ti/ccs1020/ccs/tools/compiler/ti-cgt-c6000_8.3.8" "../dss_mrr.cfg"
making package.mak (because of package.bld) ...
generating interfaces for package configPkg (because package/package.xdc.inc is older than package.xdc) ...
configuring dss_mrr.xe674 from package/cfg/dss_mrr_pe674.cfg ...
generating custom ti.sysbios library makefile ...
Starting build of library sources ...
Build of libraries failed.
subdir_rules.mk:19: recipe for target 'build-1229721713-inproc' failed
gmake: E:/Simplex-Mostafa: No such file or directory
gmake: *** No rule to make target 'E:/Simplex-Mostafa'. Stop.
error: xdc.cfg.SourceDir: "C:/ti/xdctools_3_61_02_27_core/packages/xdc/cfg/SourceDir.xs", line 209: xdc.cfg.SourceDir : Build of generated source libraries failed: exit status = 2:
js: "C:/ti/xdctools_3_61_02_27_core/packages/xdc/cfg/Main.xs", line 160: Error: Configuration failed!
gmake.exe: *** [package.mak:206: package/cfg/dss_mrr_pe674.xdl] Error 1
gmake.exe: *** Deleting file 'package/cfg/dss_mrr_pe674.xdl'
gmake.exe: *** [package/cfg/dss_mrr_pe674.xdl] Deleting file 'package/cfg/dss_mrr_pe674.h'
gmake.exe: *** [package/cfg/dss_mrr_pe674.xdl] Deleting file 'package/cfg/dss_mrr_pe674.c'
js: "C:/ti/xdctools_3_61_02_27_core/packages/xdc/tools/Cmdr.xs", line 52: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted.
gmake[2]: *** [build-1229721713-inproc] Error 1
gmake[1]: *** [build-1229721713] Error 2
gmake[1]: Target 'main-build' not remade because of errors.
gmake: *** [all] Error 2
subdir_rules.mk:16: recipe for target 'build-1229721713' failed
makefile:160: recipe for target 'all' failed
**** Build Finished ****
This is my build setting I tried to select TI v8.3.3, TI v8.3.8 and TI v8.1.3 but also gives error when I build DSS
Hi,
Please follow the steps provided in Slide 17 in the
\labs\lab0007_medium_range_radar\docs\MediumRangeRadar_DeveloperGuide.pdf
You just need to import the provided CCS projects
thank you
Cesar
Hello,
I noticed in project properties -> CCS General -> Products
Platform: ti.platforms.c6x:AWR16XX:false:600
As shown in this figure:
but I am working on AWR18XX not AWR16XX, it might that cause the problem?
I tried many versions of XDCtools, SYS/BIOS and mmWave SDK, and I still failed to build any project in Automotive toolbox 3-3-0 and 3-2-0 not only medium range radar!
Mostafa
Hello,
That problem solved and it build without error by changing to default workspace of CCS which is C:\Users\<PC's Name>\workspace_v10
but why I have to build the Radar examples in the default workspace only? Is there any way to change the workspace and still able to build radar examples successfully?
Thanks
Mostafa