My LM35CZ is exhibiting some strange behavior. The LM35 is mounted to a small PCB with a decoupling capacitor across the power pins and a 75 Ohm, 1 uF series damping network on the output. The small PCB with the LM35 is connected to a main PCB via a harness that is approximately 2 feet. The signal is filtered on the main PCB with an 10k-1uF filter before it is amplified with a non inverting OPA2188. At room temperature the output from the LM35 is only 180 mV (ie 18 C) when the room temperature is 22 C. In addition the output from the LM35 appears to be oscillating or very, very noisy. When A disconnect the harness and power it locally and measure it locally the output voltage is about 220 mV corresponding to 22C and the signal looks clean on a scope.
Any ideas as to what my problem my be?
--hk