Tool/software: TI C/C++ Compiler
My client want to have a higher angle resolution.
So I try to change the size of azimuth FFT in aoaprochwa.h(C:\ti\mmwave_sdk_03_02_00_04\packages\ti\datapath\dpc\dpu\aoaproc).
I adjusted DPU_AOAPROCHWA_LOG2_NUM_ANGLE_BINS to 7. Then, the Size of azimuth FFT will be 128.
Bug it will be crashed when I start the project.
Are there any settings that need to be modified?
For example : L2 RAM, HSRAM or L3 RAM.
What do I need to set up?
Regards,
JuiYang