Hi,
Our customers refer to the following application notes.
And they are evaluating.
LDC1000 LDC1001 LDC1041 LDC1051Evaluation module.pdf
LDC1000LDC1041LDC1051 Evaluation Module snau150a.pdf
LDC1000EVM Quick Start Guide.pdf
Then, could you tell me the difference between "Inductive Sensing GUI" and "Sensing Solutions EVM GUI".
Q1:
"Inductive Sensing GUI" has a resonance frequency of 20% or less. Is this setting unnecessary in "Sensing Solutions EVM GUI"?
Q2:
I understand that the adjustment method of Rp_MAX and Rp_MIN is the same in "Inductive Sensing GUI" and "Sensing Solutions EVM GUI".
Is that correct?
Q3:
What frequency of the sensor coil is measured by Proximity, Rp, and Frequency Inductance in “measurements” of “Sensing Solutions EVM GUI”?
Is it the point of maximum resonance frequency of the sensor coil? Or is it the point of the maximum frequency x 0.8?
The coil used is "46mm, 40 turns, 8mil trace, 6mil spacing, 4 layers" in the file below.
LDC Reference Coils User’s Guidesnou136.pdf
Best regards,
Yuto Sakai