D- is connected to GND internally? why the measured resistance between D- and Pin 6 is not zero, about 1ohm.
so if I connect D+ to D-, it have the same performance with only D+ connected to GND and D- Pin is NC?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
D- is connected to GND internally? why the measured resistance between D- and Pin 6 is not zero, about 1ohm.
so if I connect D+ to D-, it have the same performance with only D+ connected to GND and D- Pin is NC?
Hi,
If you connect the D+ and D- pin to each other you will not be able to measure a remote temperature value. If you are only using the TMP461 as a local temperature sensor, you will not see a loss of local temperature accuracy if you connect D+ and D- together or only D+ connected to GND and D- floating.
Thanks,
David
Hi David
Yes, no request for remote function.
please explain why the resistance between D- and GND is 1ohm ,while you confirmed D- is connected to GND internally.
Thanks
Peter
Hi Peter,
There is parasitic resistance between the two pins which is probably what you are seeing.
Thanks,
David