Hello,
I have a question about leaving unused inputs floating.
The datasheet clearly states that unused inputs should be connected to D-. This is to ensure that over-temperature thresholds are needlessly triggered.
I have a design which has D+ floating on one of the inputs. This channel is unused.
A few questions:
1. Can I ignore errors at startup and then disable the open-channel via the configuration registers?
2. Will the open channel impact measurement accuracy on other channels when disabled?
3. Is there anything else I should be concerned about?
Don