I am considering using a SN74CB3Q3253RGYR mux/demux in a design, but only need to use section 1, I do not need section 2. What are recommended connections for the unused pins in section 2 (A, B1 -B4, I realize 2OEn should be tied to VDD)? Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am considering using a SN74CB3Q3253RGYR mux/demux in a design, but only need to use section 1, I do not need section 2. What are recommended connections for the unused pins in section 2 (A, B1 -B4, I realize 2OEn should be tied to VDD)? Thanks.
Hi N. Maris,
A, B1-B4 - All of these terminated with 50 Ohm Resistors to ground if unused. I am not sure why we put that section in there under 9.2 because generally speaking if its an I/O pin and unused you tie it to ground with a 50 resistor for higher speed applications where reflections are a concern and can typically leave them floating otherwise. This part isn't special and operates with that idea as well .
2/OE - You are correct tie this high to disable that block.
All this information can also be found in our precision lab video on what to do with unused mux pins: https://training.ti.com/ti-precision-labs-switches-and-muxes-can-i-leave-unused-pins-floating
If you have any other questions please let me know!
Best,
Parker Dodson