Hi,
I am currently using TMUX1072DGSR as the 2:1 MUX part. Do you have any 2:1 Mux part with the tristate option?
Regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Pull /OE high. Or what do you mean with "tristate"?
Hi Abhijith,
The TMUX1072 is an analog switch so there isn't defined outputs as you'd find in a digital multiplexer - most of TI's switches/multiplexers are analog so they they have a continuous band of outputs within the operating range and the switch can be open, closed, or high impedance -> but the switch itself is passive and doesn't drive anything.
That being said - I am adding in our Logic Product line because I believe they may have a few digital multiplexers that could potentially work- but it may be limited.
Best,
Parker Dodson
If you're looking for a digital mux, you could use SN74HC257, which has 3-state outputs.