Other Parts Discussed in Thread: SN74CB3Q3384A, SN74CBTLV3861
Hi,
I am looking to use the SN74CB3Q6800PW bus switch IC with a PCI bus to allow for 3.3V and 5V IO voltages to be used in a new design.
Looking through the datasheet, it looks like BIASV can be tied to Vcc, ground or left open. I am wondering if each configuration is meant for a different purpose and if so, what would be the recommended configuration for my purposes?
Also, in the test circuit provided (Page 7) in the datasheet:
- a 50 ohm resistor is used on the Vin and Vi lines.
- Is a 50 ohm resistor going to be required for each Vi line?
- a capacitor (Cl) and two resistors (Rl) are used on the Vo lines.
- Are these required for each Vo line?
Is there an application note that gives a sample circuit?
Thank you,