Other Parts Discussed in Thread: TMUX1248
Hi Sir:
I have a application which needs switch 8MHz and 24 MHz clock signal. Does SN74LCV3157 meet this application ??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir:
I have a application which needs switch 8MHz and 24 MHz clock signal. Does SN74LCV3157 meet this application ??
This device has a specified bandwidth of 340 MHz.
Hey Jim,
Yes, the SN74LVC3157 will meet your bandwidth requirements as long as the voltage is between 0 and 5V.
I would also recommend you to take a look at the TMUX1248 which is a higher performing new product. This is a drop-in match to the SN74LVC3157 with lower on resistance and logic compatible from 1.8 to 5.5V. It will include extra features such as fail-safe logic. See TI precision lab video : What is fail-safe logic?
Thanks,
Rami