Hello team,
TS5A3159A supports Powered-off protection so I think the device is protected even if a signal, for example 3.3V is applied to COM pin when there is no power supply to the device(V+).
It looks to me that the device could support the condition because test condition of ICOM(PWROFF) spec shows also up to 5.5Vcom.
However, its absolute maximum rating says COM pin needs to be lower than V+ +0.5V.
Therefore, the device cannot support below use case(V+ is come when COM pin has some signal), correct?
Please let me know if my understanding is wrong.
Best regards,