This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN3257-Q1: question

Part Number: SN3257-Q1
Other Parts Discussed in Thread: TS5A22362, TS5A22364,

Hi team.

Could sn3257 support analog audio signal? If not, which part is the suitable?

Thanks

Jiawei

  • Hi Jiawei,

    The SN3257-Q1 can support audio signals but we do offer devices specifically designed for analog audio applications. The TS5A22364 or TS5A22362 are both devices released for analog audio that have lower RON and support negative signals. The TS5A22364 is also offered in a Q1, automotive rated version if that is a requirement.

    Thanks,
    Tyler