This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX1248: Will the outputs be diconnected when VDD is off?

Part Number: TMUX1248
Other Parts Discussed in Thread: TS5A3160, TS5A3359, TS5A3154

Hello,

I'd like to use TMUX1248 to achived 3 gain options for a amplifier.

Low gain = 1+1/10k

Mid gain = 1+1/(1/10+1/2.7)

High gain = 1+1/(1/10+1/0.68)

Will the output S1 & S2 disconnect when VDD is 0V as above pic shown? so that it can be in low gain state.

If it's not. Are there any other IC options for this purpose? 

Thank you very much.