Other Parts Discussed in Thread: TS3A5018, , TMUX1574, TMUX1134, TMUX1575
Is TS3A5018RGYR a suitable alternate for TS3A44159RGTR? If not, can you recommend one? Recommendation could be either component with less or more capability or functionality.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Michael,
You are correct that the ts3a5018 is a suitable replacement, however it has less functionality than the TS3A44159.
What features are you looking to have in a potential replacement device? Are features like 1.8v compatible control inputs important to you?
Thanks and Regards,
Kameron
TS3A44159 is in an existing design and am also looking for it to be a form/fit replacement. Dont think this is a form/fit replacement.
Hi Michael,
If you are looking for another Pin to Pin part, then we do not have one. However, some alternatives I can suggest with similar functionality are the TMUX1574, TMUX1575 (similar to the TMUX1574, but in a WCSP package), and the TMUX1134. But also the ts3a5018 is another device you could try.
Hopefully this helps you!
Thanks and Regards,
Kameron