Other Parts Discussed in Thread: ISO7041-Q1, , SN74LV125A-Q1, SN54LVTH244A-SP
Hello,
I am working on the subsystem for the CubeSat, where reliability is high importance. I am coming to You with a trateoff that I have to make.
For example, I have SPI bus between uC and FRAM chip. FRAM chip is supplied with VDD_FRAM (supplied through LCL), and uC is supplied through another LCL to get VDD.
When FRAM is not used, I want to cut off it from the SPI bus. I am thinking about two options:
a) ISO7041-Q1 use this digital isolator for the signal lines. GND is common and both power pins are connected to VDD_FRAM. It will be powered off when FRAM is not active.
b) use SN3257-Q1 switch. It will be supplied from VDD_FRAM and in default output A will be floating (disconnected from SPI bus). When powered on and SEL pin activated, it will switch to output B which will connect SPI. This model has "power-off" protection.
Which option is more reliable in this application? Note that because it's made in CMOS technology, I need to keep these IC's turned off most of the time to avoid influence of SEE (caused by radiation).
Best regards!
Slawek