This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'm confued about Vs/Vd(Source or drain voltage (Sx, Dx)). If the TMUX7212 is unpowered, there is a risk of damaging the device when the I/O voltage exceeds the VDD/VSS supplies by more than 0.5V. How to understand VDD/VSS maximum value. Based on datasheet, that is to say the device will damage if exceeds 48.5V/-48.5V? if VDD/VSS powered with ±15V, What's the maxiumum value for Vs/Vd(Source or drain voltage (Sx, Dx))? it can be calmped by internal diode to ±15V, if there are ±45V pulse input for Source or drain voltage (Sx, Dx),I want to know if diode-calmped will be damaged. Looking forward to your reply ASAP.
Thanks in advance.
Best regards.
Hello,
1.Yes if the device is unpowered and voltage are present on io pins there is a risk of damaging the device. To prevent this some of Ti's multiplexers have a feature called power off protection
2. Additionally, this device also lacks a feature called overvoltage protection which makes sure no damage happens to the device if the voltage on the io pins exceeds the supply(vdd/vss) voltage (when vdd is supplied power.)
3.Yes permanent damage can occur if the device exceeds the abs max ratings (ex.+-48.5v supplies). In addition VDD and VSS can be any value as long as 4.5 V ≤ (VDD – VSS) ≤ 44 V, and the minimum VDD is met.
4.This device can pass any signals from vss to vdd. so -15v to 15v if vdd/vss is powered +/-15v.
5.No you will need an overvoltage protection device for this
it can be calmped by internal diode to ±15V, if there are ±45V pulse input for Source or drain voltage (Sx, Dx),I want to know if diode-calmped will be damaged. Looking forward to your reply ASAP.
Can you please tell me more about your application so I can help more.
Regards
Hello,
Thanks for your support.
Currently we powered deviice with ±15V, but input voltage of Sx pin will up to ±45V. I want to know if overvoltage protection can make sure no damage happen to device? Pls help to check TMUX8212 if it is ok on this condition. thanks.
Hello Jie,
For this application please use the TMUX7412F which will have the overvoltage protection. It can be powered to +-15v supply and protect against +-45v on s pin
Please let me know if you have any further questions!