Other Parts Discussed in Thread: SN74LVC1G3157
Hi team,
customer has a 3.3V 4MHz and a 1.8V 37.125MHz clock signal need to switch. I was wondering if TS5A3159A can work here. If not, any recommended device for it?
Rayna
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
customer has a 3.3V 4MHz and a 1.8V 37.125MHz clock signal need to switch. I was wondering if TS5A3159A can work here. If not, any recommended device for it?
Rayna
Hello Rayna,
I would recommend the SN74LVC1G3157 It can support up to 300MHz and the customer trying to send a clock signal of 37MHz. A good estimation is 5x the frequency of the application. For this use case 37 x 5 = 185MHz, which the SN74LVC1G3157 can support.
For more information regarding this topic, please feel free to check out our FAQ: https://e2e.ti.com/support/switches-multiplexers-group/switches-multiplexers/f/switches-multiplexers-forum/1025430/faq-how-do-i-select-the-right-analog-switch-multiplexer-bandwidth-based-on-the-data-rate-of-my-protocol
Thanks,
Nir