Tool/software:
Hi TI-Team
I nee to bridge a 4-20mA current loop analog frontend under fault conditions. Under normal conditions VD and VSS present the MUX has nearly no impact on the current loop which is awesome. But if the MUX has no supply I'm not so sure about the values in the Datasheet. Under 7.9 Fault Conditions its says +/-125uA with VD = VSS = 0V on the Sx pins but on the Dx pins its +/-90nA. To my Understanding the Sx pins are OVP and the Dx pins are not. Why is there so much current going through the protected Sx pins?
Can I use this MUX to bridge my current loop frontends?
Thank you in advance!
Regards Theo