Hi,
I'm using (or ~probably~ misusing :) a TS5A3160 to switch a 0 to 1.5V voltage to the base of two transistors:
I change the value on the 0-1.5V input and then switch the 3160. This is done at a 1kHz rate. I'm not always getting clean switching as there is glitching between the two values meant for the separate transistor bases. BTW, I do not have a scope but the device let's me plot the transistor currents.
Please note that PE2 is a direct output from a Stellaris MCU. This output can be configured a number of ways, pullup, pulldown and differing drive currents.
I am wondering if my very simple implementation needs some type of discrete Rs or Cs to get it to function properly.
As well, please comment on whether this is better handled with a few discrete FETs as it is a very slow circuit, 1kHz.
Thanks in advance for your help!
Kind regards,
Kevin Kreger