Dear Sir
May I know TS3USB3031 support 1 to 3 MUX for UART interface ??
As I know TS5A23157 may could support 1 to 2 Mux for UART
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir
May I know TS3USB3031 support 1 to 3 MUX for UART interface ??
As I know TS5A23157 may could support 1 to 2 Mux for UART
Thanks
Kai,
All of our switches can be used for any application as long as the signal you are attempting to pass through the switch is within the recommended operating conditions. The TS3USB3031 is a 2 channel 1:3 mux with 6.5 GHz bandwidth and supports signals 0-3.6 V.
If you look at this e2e post below you will see that UART signals could be supported by the TS3USB3031 as they have signals that are within the recommended operating conditions of the device.
Thank you,
Adam