The datasheet indicates that the part performance specifications are qualified up to +85 deg C (Ambient). The question is, what is a max allowable Die junction temperature under normal operation? Is it capable of higher temp (say up to 125 Deg C Junction Temp) assuming not much power is being dissipated by the switch currents flowing through the part? Or is there some other concern about exceeding 85 deg C?