The Recommended Operating Conditions table says the supply voltage VDD can be as low as 3V. I'd like to use this device with a 3.3V supply. What are the on/off conditions for the control input Vc with a 3.3V supply? That is, how high does my Vc input have to be to connect the switch, and how low does my Vc input have to be to disconnect the switch?