This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS5A12301E: TS5A12301E use as a load switch.

Part Number: TS5A12301E

Hi sir:

    TS5A12301E  be used as  Bidirection load Switch. If the Current form Com to NC(NO) Under 0.4 A.Is it?

It means The com I will connect to Power,the NC(No) will connect to load. Or Nc(No) connect the power, the com connect the load.