This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS5A3160: Using a TS5A3160 to swtich a RS485 bus line

Part Number: TS5A3160

Hi,

I'm using a TS5A3160 to switch a RS485 bus line however it isn't working as I expected. Yellow and pink plots are Line A of RS485 bus, pink is from node 1 and yellow from node 2. Switch is between node 1 and 2.

After the first master command, the switch change it's position (blue plot is the IN line of TS5A3160). The second command of master arrived at node 2 (yellow) with some signal malfunction however it is sufficient for it to recognized the command and answer to the command.

Can you help me identify the problem?