Hi Team,
SN74CBT3251 was used in customer. The input PinB1~ B7 was shorted TO ground randomly when SN74CBT3251 was used to sample temperature.Here is the schematic for SN74CBT3251. The failure rate is 2%.
This is a special application, B1 is NC, the rest B2~B8 connect to NTC, When MCU control enable pin to open the path, NTC is pulled up by the pin A.
We also test the power sequence for this application, 5V is powered up first. Could you give us some advice? Thanks.
BR
Songzhen Guo