Hi TI EE:
Please help me to make sure if the below diagram is working or not.
Both SPI interfaces and SEL, /EN are running @ 3.3V Logic level ,while the VDD of TMUX1574 VDD is 5V.
BR
Cheney_Sun
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI EE:
Please help me to make sure if the below diagram is working or not.
Both SPI interfaces and SEL, /EN are running @ 3.3V Logic level ,while the VDD of TMUX1574 VDD is 5V.
BR
Cheney_Sun
Hi Cheney_Sun,
The TMUX1574 operates at consistent thresholds for it's logic, this is why it is 1.8V compatible. I've attached the logic levels from pg. 6 of the TMUX1574 datasheet below (VDD range shown here: 1.5V-5.5V) :
For the TMUX1574 to register a logic high, the minimum voltage on the select pin, with reference to ground, is 1.2V; while the maximum voltage on the select pin to register a logic low is 0.45V. So as long as the MCU at 3.3V has a VOH >= 1.2V and a VOL <= 0.45V you shouldn't have issues with the application.
For more information on logic levels in our MUX's as well as 1.8V logic compatibility please see our Precision Lab Video here and an App Note on 1.8V logic here.
Best Regards,
Parker Dodson
Hi Clemes Ladisch:
Thank you for your reply.Your answer is different with above Parker Dodson's answer.Which one is right?TKS~
BR
Cheney_Sun
Hi Parker Dodson:
Thank you for your reply.Your answer is different with below Clemens Ladisch's answer.Which one is right?TKS~
BR
Cheney_Sun
Both answers say "yes", with varying levels of detail. Nothing in them is contradictory; both are right.
To allow us to remove any misunderstandings: which point do you think is different?
Hi Cheney_Sun,
Your application as indicated by your diagram should work fine.
I agree with what Clemens said, but if you need clarification on any of those points please ask!
The TMUX1574 is 1.8V compatible. This means that it can be controlled by a MCU that is running off of 1.8V source up to 5.5V.
The MCU you are working with is at 3.3V. So if the GPIOs controlling the switch have an Output high of greater or equal to 1.2V and an output low less than or equal to 0.45V the system will behave as expected.
The switch at 5V VDD can handle VDD x 2 at the input and output a max of VDD. For your application of a 3.3V system at a 5VDD, there should be no issue with the signals passing through the switch.
If there is anything else I can clarify please let me know.
Best Regards,
Parker Dodson