This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear SIrs,
Is there any solution that similar with SN74LV4051A(1 channel 8:1 mux/demux) but with output latch function.
The output will keep last state unless it changed.
Thanks.
Sorry and let me explain it!
Since I can use COM pin as input and Yn pins as output, what I want is, at the 1st time, I choose Y0 on and the output is high, then I choose Y6 on and output is low, but I need Y0 keeps "HIGH" untill I choose and changed it.
If after 2nd time, I choose Y7 on, then output low, what I want to get are: Y0=high, Y6=low, and Y7=low, and so on.
Hey Peter,
As Clemens mentioned this is a passive switch so the SN74LV4051A won't be able to provide this function. I'm going to loop in the logic team to see if we can find you the right fit.
Rami
Thanks Rami!
Hi Peter,
I feel Clemens offered a great device option to achieve the desired functionality. Let me know if the SN74HC259 function is what you are after.