This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear TI,
I Attach a schematics file.
Please Review & Comment.
Thank you.
Best Regards,
Inho Jeon
Hey Inho Jeon
I've taken a look and the layout checks out with the only comment being that the R527 resistor can be DNI as well. There isn't a need for a pulldown resistor on the Enable since there is an internal pulldown on the TMUX1574 logic pins.
Other than that everything looks fine. With 3V Vdd the device can handle up to 6 volts through the I/O so that should work fine for SPI signals, which I believe at 3.3V. In case I've missed the voltage level, just make sure to note that the powered-off protection (isolation when Vdd<1.5V) only goes up to 3.6V on the signal paths.
Let me know if there's anything else you need,
Rami
Inho,
Yes, this is okay and you're correct in your statement.
Let me know if there's anything else you may have a question about
Thanks,
Rami