Tool/software: TI C/C++ Compiler
Hi
I need to set up a different clock for the same input
Say currently I am generating 150MHz clock which variable setting will allow me to generate different clocks like 100MHz, 70MHz or 50MHz
Regards
Uzmeed
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TI C/C++ Compiler
Hi
I need to set up a different clock for the same input
Say currently I am generating 150MHz clock which variable setting will allow me to generate different clocks like 100MHz, 70MHz or 50MHz
Regards
Uzmeed
Hello Uzmeed,
Do you already have a configuration for this device? Assuming you have programmed a VCO frequency of 3000 MHz, then the only field that needs to be re-programmed is the clock divider. For example, if CLKout0 = 150 MHz from a 3000 MHz VCO, then CLKout0_DIV in register R0[15:5] must be set = 20.
Anytime you change the divider, it is possible for the phase of the output clock to change with respect to the other clocks. If required you can re-SYNC the output dividers.