Hi,
I am using usB jtag emulator in TMS320DM6437 EVM board .
After debuging active project iam getting this error.
C64XP_0: Trouble Setting Breakpoint with the Action "Finish Auto Run" at 0x6580: Error 0x0000000A/-1176 Error during: Memory, Break Point, The IM memory request is not serviced by the HW memory system. This could be caused by the memory address specified does not exist in the specified memory/cache level.
C64XP_0: Trouble Setting Breakpoint with the Action "Process CIO" at 0x6578: Error 0x0000000A/-1176 Error during: Memory, Break Point, The IM memory request is not serviced by the HW memory system. This could be caused by the memory address specified does not exist in the specified memory/cache level.
C64XP_0: Trouble Setting Breakpoint with the Action "Terminate Program Execu
i wrote a simplecode for averageing no's. no break point .
what is the solution for these error.