This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have got one license from CCSV4, load one project, and have passed the compiling, see below picture
But when I do the debug operation, it will show one window to register again, and this software state has change to "unlicensed”, see below picture
I don't know why, who can help me to solve this problem, thanks very much!!!
Hi Kent,
could you please provide a bit further detail on your setup?
- What CCS version are you using (Note a v4 license will not work with v5. These are licensed separately) If you have a valid subscription or are using the XDS100 for example you should be able to freely migrate to v5.
- What type of license have you been/are you using? How have you set this license up?
- What target/hardware do you use?
Best Regards,
LIsa
#Please Do not delete this comment line. INCREMENT CCS_LINKER_FULL tidspssw 4.99 permanent uncounted \ VENDOR_STRING="Not Used" HOSTID=d4bed915c420 ISSUER="Texas \ Instruments Inc." \ SN=CustomFID_84F759A0_C013_11E1_923E_C4399AA829B0 \ START=25-jun-2012 TS_OK SIGN="0061 B3A9 5AB9 1EA9 33A6 D5A2 \ 9091 B500 41E6 1D04 C1D8 EADC 271F 3509 C822" INCREMENT CCS_ISA_ALL tidspssw 4.99 permanent uncounted \ VENDOR_STRING="Not Used" HOSTID=d4bed915c420 ISSUER="Texas \ Instruments Inc." \ SN=CustomFID_84F759A0_C013_11E1_923E_C4399AA829B0 \ START=25-jun-2012 TS_OK SIGN="0075 832C 8C59 FAA3 B5AD 067B \ 390D 7A00 6796 1EB9 8F0F 52CB 33B4 2546 CA25" INCREMENT CCS_CONNECTION_RESTRICTED tidspssw 4.99 permanent uncounted \ VENDOR_STRING="Not Used" HOSTID=d4bed915c420 ISSUER="Texas \ Instruments Inc." \ SN=CustomFID_84F759A0_C013_11E1_923E_C4399AA829B0 \ START=25-jun-2012 TS_OK SIGN="00DB D4AA 2855 823F 77E4 481C \ 74ED E100 F37E 1691 AA8D 563F 1F2D 929E 5FC2" INCREMENT CCS_DEBUGGER tidspssw 4.99 permanent uncounted \ VENDOR_STRING="Not Used" HOSTID=d4bed915c420 ISSUER="Texas \ Instruments Inc." \ SN=CustomFID_84F759A0_C013_11E1_923E_C4399AA829B0 \ START=25-jun-2012 TS_OK SIGN="0018 6AA3 7287 6196 92F5 CF24 \ 512E D000 6645 5504 E59F 36F7 1260 C3EA 371D"
- CCS Version: 4.2.5.00005
- has attched licensed file, file type has changed to *.txt for this web server limitation, you can replaced it to *.lic
- use Signum debug tool(JET - C2000), and used simulated board of SEED_DEC2812, DSP chip is TMS320F2812.
- Also when I debug one project, it will alarm the error message, listed below picture.
Any question, please call my office tel:+86 051262620466
Thanks for your reply
Hi Kent,
so are you using the free limited license? This will not work with the SEED emulator. Have you ever used the trial license? Could you please try that if not or contact me with a friend request so I can send you a 30 day trial license. Do you remember what you set up the very first time you ran CCS? I assume you do not have a purchased license?
Best Regards,
Lisa
I actived this license from your TI web site, the speed is not so fast when I run the CCS, and it has show licensed state of this CCS, I don't know why.
Could you send me the trial license again to try it . thanks .
HI Kent,
could you please explain in more detail exactly what you are doing? Did you purchase a license? So not using SEED it shows licensed? I am not sure what you mean here. Do you mean you originally had a trial license? Did it expire?
Best Regards,
Lisa
I didn't have trial license before, if possible, could you please send me one trial license, I want to check it in my computer and CCS, to understand what's problem there, the license I have now is send by third part, we purchase their some simulated tool.
Hi Kent,
ok, I will send you a time limited trial offline for you to double check licensing. I sent a friend request so that we can share files offline.
Best Regards,
LIsa
Hi Kent,
ok, glad to hear and all the best with development.
Best Regards,
LIsa