This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
My name is Marcelino Martinez. I installed a floating license server on a computer running Linux, (Ubunto) but now I have to move this license to a new computer. I rehosted and generatee a new license file for the new computer. Due to an error I used a secondary MAC of this computer so the license file was not valid. TI does not allow to rehost to a new MAC address, so I contacted TI support and they change the MAC to the correct one. This way I can generate a new license, but following the tutorial http://processors.wiki.ti.com/index.php/License_Server_Administration_for_CCS#UNIX:_command_line_setup I can not start the license server. (I used this manual the fist time I install the license server)
I have checked the MAC addres of the computer with ifconfig. This is the answer:
eth0 Link encap:Ethernet direcciónHW 00:30:48:7e:9f:90
Direc. inet:147.156.27.176 Difus.:147.156.27.255 Másc:255.255.254.0
Dirección inet6: 2001:720:1014:26:230:48ff:fe7e:9f90/64 Alcance:Global
Dirección inet6: fe80::230:48ff:fe7e:9f90/64 Alcance:Enlace
ACTIVO DIFUSIÓN FUNCIONANDO MULTICAST MTU:1500 Métrica:1
Paquetes RX:2308874043 errores:0 perdidos:0 overruns:0 frame:0
Paquetes TX:3313955507 errores:0 perdidos:0 overruns:0 carrier:0
colisiones:0 long.colaTX:1000
Bytes RX:723517339559 (723.5 GB) TX bytes:4110979218505 (4.1 TB)
Memoria:f8420000-f8440000
I have checked the license file, and it seems the MAC is OK. :
Fulfillment ID: CustomFID_534D10F0_604E_11E0_8007_A384D961BBDA
Activation ID : F4D4-40C0-A40B-11DE-B147-F3DF-F8F4-B6EC
Product Name : CCSTUDIO TMDSCCS-ALLUNVF100
Product Version : 4.x
Activation Date : Apr 6, 2011
Start Date : May 27, 2010
Expiration Date : PERMANENT
Fulfillment Count : 100
Overdraft Count : 0
Server Ids : VENDOR_DEFINED=0030487E9F90,
Node Locked Ids :
License Model Name : DSP-FLT-Perm-CCS
License Model Attributes :
But when I check the state of the license:
Using ./lmutil lmstat -a
Flexible License Manager status on Thu 4/7/2011 00:34
License server status: 27000@hiperion
License file(s) on hiperion: /opt/license_server/licenses/TMDSCCS-ALLUNVF100-v4.0.lic:
hiperion: license server UP (MASTER) v11.9
Vendor daemon status (on hiperion):
tidspssw: The desired vendor daemon is down. (-97,121)
I have reread the licence, I have starting the installation from scratch, but I always got the same results. Please could you give me any advice ?
Regards
Marcelino,
What are the contents of the log files? The FlexLM Administrator's Guide does not give much more information about error -97 apart from:
The desired vendor daemon is down.
1) Check the lmadmin or lmgrd log file, or 2) Try lmreread.
Also, check if your .LIC file matches the MAC Address: the following lines should be at the beginning of the file:
License File said:#Please do not delete this comment line.
SERVER this_host 0030487E9F90
VENDOR tidspssw
Hope this helps,
Rafael
I have already try what you proposed. The MAC is the same. I have also reread the license but I always have the same error.
Thanks