I'm using CCS version 11.1.0.00011. I'm trying to create a static lib. From the pulldown menus I select "File", then "New" then "CCS Project". See below for the settings I chose. I click "Finish" and the project is created. I then go to project Properties for the project (FooLib) and when clicking the "Build" property I get the message shown in the second image below "The currently displayed page contains invalid values".
Is this a bug???