Hey there,
I seem to be having some CCS build issues.
I am working with some others to run and edit the WIFI SDK Cloud OTA example in an attempt to integrate OTA updates into our wireless microcontroller network. I have run this example in the past with great success, but now I seem to be having problems.
One of my partners has been able to import and build the example just fine on his Windows machine, but any time I import it on a new machine from the SDK, I get the SDK-related errors below. He has sent me a zip of his working project as well as shared with me on GitHub, which both just throw the same errors. When I try to import on Linux or Windows machines, I get the same errors.
We have the same software setups for Windows machines: Windows 11, CCC 12, WIFI SDK 4.10.00.10, 432 SDK 3.40.01.02.
Thanks in advance for any advice,
Greg