This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C2000Ware SDK for MacOS --- Installer is damaged(or corrupted) as provided by TI download site

Other Parts Discussed in Thread: C2000WARE

After downloading from the official TI repository for MacOS (https://www.ti.com/tool/C2000WARE?keyMatch=C2000WARE%20DOWNLOAD#downloads) , upon starting the install I see this error :

The C2000Ware MACOS Installer is broken in some way and will not install. I have tried 2x now to download and install, and receive the same error.  Can someone at TI config the problem ?  Can you please check my md5sum to see if it matches the file as provided from the download site ?

(base) beadon@blade Downloads % md5 C2000Ware_5_00_00_00_setup.app.tar.gz

MD5 (C2000Ware_5_00_00_00_setup.app.tar.gz) = 136d6b0f8654adc35935c1582dffc4ed

(base) beadon@blade Downloads % tar -zxvf C2000Ware_5_00_00_00_setup.app.tar.gz

x C2000Ware_5_00_00_00_setup.app/

x C2000Ware_5_00_00_00_setup.app/Contents/

x C2000Ware_5_00_00_00_setup.app/Contents/_CodeSignature/

x C2000Ware_5_00_00_00_setup.app/Contents/_CodeSignature/CodeDirectory

x C2000Ware_5_00_00_00_setup.app/Contents/_CodeSignature/CodeRequirements

x C2000Ware_5_00_00_00_setup.app/Contents/_CodeSignature/CodeSignature

x C2000Ware_5_00_00_00_setup.app/Contents/_CodeSignature/CodeResources

x C2000Ware_5_00_00_00_setup.app/Contents/Info.plist

x C2000Ware_5_00_00_00_setup.app/Contents/Resources/

x C2000Ware_5_00_00_00_setup.app/Contents/Resources/osx-x86_64.dat

x C2000Ware_5_00_00_00_setup.app/Contents/Resources/installbuilder.icns

x C2000Ware_5_00_00_00_setup.app/Contents/Resources/installbuilder

x C2000Ware_5_00_00_00_setup.app/Contents/MacOS/

x C2000Ware_5_00_00_00_setup.app/Contents/MacOS/installbuilder.sh

x C2000Ware_5_00_00_00_setup.app/Contents/MacOS/osx-x86_64

Further details of the download and extraction --

(base) beadon@blade Downloads % ls -latrh C2000Ware_5_00_00_00_setup.app*

-rw-r--r--@ 1 beadon  staff   362M Oct 17 20:43 C2000Ware_5_00_00_00_setup.app.tar.gz

C2000Ware_5_00_00_00_setup.app:

total 0

drwxr-xr-x@    3 beadon  staff    96B Jul 14 02:08 .

drwxr-xr-x@    6 beadon  staff   192B Jul 14 02:12 Contents

drwx------@ 1169 beadon  staff    37K Oct 17 20:43 ..

Context -- MacOS is using the Intel CPU. (serial number hidden)

  • Hi, 

    When an application gets downloaded from any source other than those that Apple seems suited, the application gets an extended attribute "com.apple.Quarantine". This triggers the message: "<application> is damaged and can't be opened. You should move it to the Bin."

    Remove the attribute and you can launch the C2000Ware installer .

    To do this, open a terminal and type:$ xattr -c <path/to/C2000Ware_5_00_00_00_setup.app>

    Pls try this out and let us know if it resolves the issue.

    Best Regards

    Siddharth

  • wow, yes, that fixed it.

    Have you considered packaging this as a .dmg file instead of the tar.gz to avoid this ?