Other Parts Discussed in Thread: SYSBIOS
I have installed the SDK and CCS afresh. I use the resource explorer to import "rfPacketRX". When I try to "clean" the project, I get a pop-up which says that rm.exe could not launch correctly.
If I proceed with a "rebuild" of the project, I get the output below. It seems sh.exe is failing.
Which rm.exe and sh.exe should be called, and how can I ensure that the correct versions are being used?
But maybe there is something else causing this?
BTW, when I did the same thing using OSX, it worked fine. But I need this to work under Windows.
Build output:
**** Clean-only build of configuration Debug for project tirtos_builds_CC1310_LAUNCHXL_release_ccs ****
"C:\\ti\\ccs1250\\ccs\\utils\\bin\\gmake" -k -j 4 clean -O
DEL /F "tirtos_builds_CC1310_LAUNCHXL_release_ccs.lib" "configPkg\linker.cmd" "configPkg\compiler.opt"
RMDIR /S/Q "configPkg\"
Could Not Find C:\Users\markuswallgren\workspace_markus\tirtos_builds_CC1310_LAUNCHXL_release_ccs\Debug\tirtos_builds_CC1310_LAUNCHXL_release_ccs.lib
Could Not Find C:\Users\markuswallgren\workspace_markus\tirtos_builds_CC1310_LAUNCHXL_release_ccs\Debug\configPkg\linker.cmd
Finished clean
**** Build Finished ****
**** Build of configuration Debug for project tirtos_builds_CC1310_LAUNCHXL_release_ccs ****
"C:\\ti\\ccs1250\\ccs\\utils\\bin\\gmake" -k -j 4 all -O
Building file: "../release.cfg"
Invoking: XDCtools
"C:/ti/ccs1250/xdctools_3_62_01_16_core/xs" --xdcpath="C:/ti/simplelink_cc13x0_sdk_4_20_02_07/source;C:/ti/simplelink_cc13x0_sdk_4_20_02_07/kernel/tirtos/packages;" xdc.tools.configuro -o configPkg -t ti.targets.arm.elf.M3 -p ti.platforms.simplelink:CC1310F128 -r release -c "C:/ti/ccs1250/ccs/tools/compiler/ti-cgt-arm_20.2.7.LTS" --compileOptions " -DDeviceFamily_CC13X0 " "../release.cfg"
making package.mak (because of package.bld) ...
generating interfaces for package configPkg (because package/package.xdc.inc is older than package.xdc) ...
configuring release.xem3 from package/cfg/release_pem3.cfg ...
generating custom ROM library makefile ...
Starting build of library sources ...
making C:/Users/markuswallgren/workspace_markus/tirtos_builds_CC1310_LAUNCHXL_release_ccs/src/sysbios/rom_sysbios.aem3 ...
clem3 C:/ti/simplelink_cc13x0_sdk_4_20_02_07/kernel/tirtos/packages/ti/sysbios/BIOS.c ...
Build of libraries failed.
subdir_rules.mk:12: recipe for target 'build-1317695535-inproc' failed
0 [main] sh.exe" 372 sync_with_child: child 7084(0x244) died before initialization with status code 0xC0000142
34 [main] sh.exe" 372 sync_with_child: *** child state waiting for longjmp
C:/Users/MARKUS~1/AppData/Local/Temp/make2932-3.sh: fork: Resource temporarily unavailable
gmake[1]: *** [makefile:61: rom_sysbios.obj] Error 128
gmake: *** [C:/Users/markuswallgren/workspace_markus/tirtos_builds_CC1310_LAUNCHXL_release_ccs/src/makefile.libs:57: C:/Users/markuswallgren/workspace_markus/tirtos_builds_CC1310_LAUNCHXL_release_ccs/src/sysbios/rom_sysbios.aem3] Error 2
error: xdc.cfg.SourceDir: "C:/ti/ccs1250/xdctools_3_62_01_16_core/packages/xdc/cfg/SourceDir.xs", line 211: xdc.cfg.SourceDir : Build of generated source libraries failed: exit status = 2:
js: "C:/ti/ccs1250/xdctools_3_62_01_16_core/packages/xdc/cfg/Main.xs", line 160: Error: Configuration failed!
gmake.exe: *** [package.mak:202: package/cfg/release_pem3.xdl] Error 1
gmake.exe: *** Deleting file 'package/cfg/release_pem3.xdl'
gmake.exe: *** [package/cfg/release_pem3.xdl] Deleting file 'package/cfg/release_pem3.h'
gmake.exe: *** [package/cfg/release_pem3.xdl] Deleting file 'package/cfg/release_pem3.c'
js: "C:/ti/ccs1250/xdctools_3_62_01_16_core/packages/xdc/tools/Cmdr.xs", line 52: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted.
gmake[1]: *** [build-1317695535-inproc] Error 1
Building file: "../release.cfg"
Invoking: XDCtools
"C:/ti/ccs1250/xdctools_3_62_01_16_core/xs" --xdcpath="C:/ti/simplelink_cc13x0_sdk_4_20_02_07/source;C:/ti/simplelink_cc13x0_sdk_4_20_02_07/kernel/tirtos/packages;" xdc.tools.configuro -o configPkg -t ti.targets.arm.elf.M3 -p ti.platforms.simplelink:CC1310F128 -r release -c "C:/ti/ccs1250/ccs/tools/compiler/ti-cgt-arm_20.2.7.LTS" --compileOptions " -DDeviceFamily_CC13X0 " "../release.cfg"
configuring release.xem3 from package/cfg/release_pem3.cfg ...
generating custom ROM library makefile ...
Starting build of library sources ...
making C:/Users/markuswallgren/workspace_markus/tirtos_builds_CC1310_LAUNCHXL_release_ccs/src/sysbios/rom_sysbios.aem3 ...
clem3 C:/ti/simplelink_cc13x0_sdk_4_20_02_07/kernel/tirtos/packages/ti/sysbios/BIOS.c ...
Build of libraries failed.
subdir_rules.mk:12: recipe for target 'build-1317695535-inproc' failed
0 [main] sh.exe" 4444 sync_with_child: child 5300(0x248) died before initialization with status code 0xC0000142
46 [main] sh.exe" 4444 sync_with_child: *** child state waiting for longjmp
C:/Users/MARKUS~1/AppData/Local/Temp/make2808-3.sh: fork: Resource temporarily unavailable
gmake[1]: *** [makefile:61: rom_sysbios.obj] Error 128
gmake: *** [C:/Users/markuswallgren/workspace_markus/tirtos_builds_CC1310_LAUNCHXL_release_ccs/src/makefile.libs:57: C:/Users/markuswallgren/workspace_markus/tirtos_builds_CC1310_LAUNCHXL_release_ccs/src/sysbios/rom_sysbios.aem3] Error 2
error: xdc.cfg.SourceDir: "C:/ti/ccs1250/xdctools_3_62_01_16_core/packages/xdc/cfg/SourceDir.xs", line 211: xdc.cfg.SourceDir : Build of generated source libraries failed: exit status = 2:
js: "C:/ti/ccs1250/xdctools_3_62_01_16_core/packages/xdc/cfg/Main.xs", line 160: Error: Configuration failed!
xdctools_3_62_01_16_core\gmake.exe: *** [package.mak:202: package/cfg/release_pem3.xdl] Error 1
xdctools_3_62_01_16_core\gmake.exe: *** Deleting file 'package/cfg/release_pem3.xdl'
xdctools_3_62_01_16_core\gmake.exe: *** [package/cfg/release_pem3.xdl] Deleting file 'package/cfg/release_pem3.h'
xdctools_3_62_01_16_core\gmake.exe: *** [package/cfg/release_pem3.xdl] Deleting file 'package/cfg/release_pem3.c'
js: "C:/ti/ccs1250/xdctools_3_62_01_16_core/packages/xdc/tools/Cmdr.xs", line 52: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted.
gmake[2]: *** [build-1317695535-inproc] Error 1
subdir_rules.mk:9: recipe for target 'build-1317695535' failed
gmake[1]: *** [build-1317695535] Error 2
makefile:127: recipe for target 'all' failed
gmake[1]: Target 'configPkg/linker.cmd' not remade because of errors.
gmake: *** [all] Error 2
**** Build Finished ****