Part Number: UCD3138
Tool/software:
Hi team, we are working on 3 kw charger .In the 3Kw charger we have used the UCD3138RGC mcu . which debugger is best for UCD3138RGC that is supported by code Composer studio?
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: UCD3138
Tool/software:
Hi team, we are working on 3 kw charger .In the 3Kw charger we have used the UCD3138RGC mcu . which debugger is best for UCD3138RGC that is supported by code Composer studio?
Thank you
Hello Ranjeet,
While you edit and build your firmware using Code Composer Studio, you do not FLASH using CCS during the debug stage. Instead, you use the Fusion Studio GUI to flash your firmware with the USB-to-GPIO2 onto the UCD3138. Only once you are ready to flash production firmware will you attempt to use JTAG to flash firmware onto the UCD3138.
Regards,
Jonathan Wong
ok Jonathan, i will try .if face any problem then i will reach you.thank you so much
dear jonathan ,Using Fusion Studio GUI in offline mode ,can i download the firmware in mcu ?,
because i can not find any download option .kindly see attached file .

Hello Ranjeet,
As asked in your other E2E post, please confirm that you have followed the UCD3138 quickstart steps in this E2E post. The Fusion Design OFFLINE is only used as an example to see what the Fusion GUI would look like. You need to use the UCD31xx Device GUI to flash the firmware onto the UCD3138 and you use the Fusion Design Online to configure and monitor the UCD while it is operating in a power supply.
Regards,
Jonathan Wong