This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello All,
I was trying to import an existing CCS4 project to CCS5. I got the error shown below.
I had three projects to import; one of them worked successfully, the other two gave me that error.
Any ideas?
Thanks in advance,
-Quark
Hi Quark
it seems one or both of two things might be happening here
- you are importing to a version of CCS that does not have the code generation tool version used to create the project installed
- you are importing to a version of CCS that did not get support for the product family installed
Please double check and keep us informed.
Best Regards,
Lisa
I found what the problem was.
If your project had multiple build configurations under CCS v4 (especially old unused ones), some of them may still be set to use older versions of code generation tools. One should either delete all (except one) build configurations or make sure they are all updated to use a version of code generation tools that comes with CCS v5.
After that fix, import into v5 works.