With a DSP/BIOS application CCS runs tconf to generate C and assembly code. Then it compiles the generated code. How is it possible to setup other code generators with CCS?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
With a DSP/BIOS application CCS runs tconf to generate C and assembly code. Then it compiles the generated code. How is it possible to setup other code generators with CCS?
John,
There is a concept of a builder where you add a plug-in that handles building a particular type of file. We have done this for .tcf and .cfg files for building BIOS. It is possible (but a lot of work) to create other builders. However those builders would not be associated with a CCS Project. Another thing you would want to create is an error parser which would parse the output and display the errors in the problems view.
I would recommend either going with a standard make project where you can control the build from the makefile or to try to utilize a post build step that builds the other files that you want to build.
Regards,
John
By 'Post build step" under ccs v5 are you referring to: right click on project, Properties, C/C++ build, Settings, Build Steps?
I want to generate C code that is linked with hand-written C code. The pre and post build steps are not executed if the build is up to date.
I think moving the entire project to hand-written makefiles would take more time than I'm prepared to put in solve this problem. I'd rather run the code generator by hand and check its outputs in to revision control each time the inputs changed.