Hi,
We have a LogicPD Zoom OMAPL138EVM with TMS320C6748 SOM. Today I found an OLD Wintech TDS510USB Plus JTAG Emulator. I downloaded the latest driver and CCSv4.0 support files for the device from Wintech site. Driver installation was successful and is properly registered in device manager.
I created a C6000 'Hello world' project in CCSv4.2.2. In target configuration file TDS510USB Plus JTAG selected and C6748 selected and appropriate GEL file added. The program compiled successfully.
But when I launched debug, it says
Error Connecting to target
(Error-603 @ 0x0)
A Required dynamic library could not be resolved.
The library doesn't export a required function
(Release 5.0.333.0)
Content of my ccBoard0 file is
# config version=3.5
$ sepk
pod_drvr=tds510usb.dll
pod_port=0x240
$ /
$ uscif
slowclk=NO
tdoedge=RISE
$ /
@ icepick_c family=icepick_c irbits=6 drbits=1 subpaths=1
& subpath_0 address=17 default=no custom=no force=yes pseudo=no
@ c674x_0 family=tms320c64plus irbits=38 drbits=1
& /
# /
Please help......
Regards,
Dinu