This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6457:Migrating from CCSv3.3 to CCSv5

Other Parts Discussed in Thread: TMS320C6457

Hi,

 

One of my customers is working on a corporate cross-border project. The hardware platform is made by another company. On this platform they have to create signal processing software, the target processor: TMS320C6457. The hardware platform API libraries are available for communication with the environment of the TMS320C6457. These libraries were created with CCS v3.3 and not available as source code. 

They are looking for migration to CCSv5. They are aware of http://processors.wiki.ti.com/index.php/Migrating_to_CCSv5 

Would you advise to stay with CCS v3.3 for C6457? 

Can they migrate/ link to CCS v5 the old object file libs from CCS v3.3 without any problems according to compiler/linker differences?

 

Thanks and Regards,

Majda