This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am running CCS 5.1 in a linux virtual box on a Windows 7 PC. The Oracle Virtual Box is configured with a USB filter for the XDS 510USB emulator. The target is a L138 so it has both an ARM and a DSP.
When trying to connect using the emulator, it says it is trying to initialize the debugger (ICEPICK_C) and after a bit of time, there is a pop-up that says "Error initializing emulator". The title of the dialog is "Spectrum Digital XDS510USB Emulator_0/ICEPICK_C
At first, it seemed possible that it was a licensing problem and indeed, there was a licensing issue. With that solved though, the behavior is not any different.
Will the USB-based emulator work from CCS 5.1 running in a VM virtual box?
Thanks.
Hi,
John Pruitt said:Will the USB-based emulator work from CCS 5.1 running in a VM virtual box?
Unfortunately I don't think that will be possible with your emulator. Please check the section Linux as a guest OS of the page below:
http://processors.wiki.ti.com/index.php/VMware_with_CCS
Regards,
Rafael
John - sorry, there is no page for VirtualBox. The CCS team extensively uses VMware. But there are many people who are successfully using CCS with VirtualBox. Hopefully someone can share their experiences.
ki