I am using CCSv5.1 as an "Eclipse Plugin" rather than a standalone installation. Below are the versions of eclipse and ccs :
Eclipse IDE for C/C++ Developers
============================
Version: Indigo Service Release 2
Build id: 20120216-1857
Code Composer Studio
====================
Version: 5.1.0.201201061800
Build id: N201201061800
The debugged works fine . I am able to connect to target and debug without issues. However none of the options under Tools menu work.
For example on selecting "Image Analyzer" I get the following error pop up:
"The chosen operation is not currently available"
Please let me know if this issue is resolved in a later version of CCS