This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Options under Tools menu dont work when CCS installed as eclipse plugin

I am using CCSv5.1 as an "Eclipse Plugin" rather than a standalone installation. Below are the versions of eclipse and ccs :

Eclipse IDE for C/C++ Developers
============================
Version: Indigo Service Release 2
Build id: 20120216-1857

Code Composer Studio

====================
 Version: 5.1.0.201201061800
 Build id: N201201061800

The debugged works fine . I am able to connect to target and debug without issues. However none of the options under Tools menu work.

For example on selecting "Image Analyzer" I get the following error pop up:

"The chosen operation is not currently available"

Please let me know if this issue is resolved in a later version of CCS