This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS 5.2 installation problem, Win XP

Hello,

when installing CCS5.2 on a Win XP PC I get several "Installation failed" messages. Finally the installer claims : "successfully installed".

When starting CCS 5.2 I only see a bare Eclipse installation without any TI plugins.

I downloaded "ccs_setup_5.2.0.00069.exe" for installation. A previous CCS 5.1 installation was de-installed before installing CCS 5.2. (incl. re-boot).
The installer seems to be ok as a colleague did a successful installation on a brand new Win 7 PC (no CCS installed before). 

Any idea how to solve the problem ?

Best regards,
Mario

PS : I attached the InstallJammer Registry directory contents and a few screenshots ....

InstallJammer Registry.zip
  • Hi Mario,

    I suspect the issue might be I see you have used directories with spaces .. in particular Documents and Settings.

    Please try using only directories with no space or accented/special characters and keep us informed.  (Eg use only c:/ti or c:/mycccs)

    Best Regards,

    Lisa

  • Hi Lisa,

    thank you for your fast answer ..... unfortunately this did not help.

    Any other idea ?

    Best regards,
    Mario 

  • Hi Mario,

    can you please confirm what you did?  I did see it your logs it does seem the directory is the issue.  Did you try a fresh installation?  I am also wondering whether your unzip utility is using a temp directory with such a problem.  Please double check that as well.

    Best Regards,

    Lisa

  • Hi Mario,

    could you please confirm what you tried that you say the tips did not help?   Some further details would really help us here.

    Best Regards,
    Lisa

  • Hi Mario,

    Do you have an unzip program on your path? It looks like the installer cannot find the unzip utility or it's corrupted (see error in log below). Please make sure there's a valid unzip utility on the path before running the install. I hope this helps.

    couldn't unzip idebuildRepo.zip: The system cannot execute the specified program.

    Danish Innis

  • Lisa, Danish,

    there is an unzip in the PATH and the installer is located in a directory without spaces ......

    Anyway unzip caused this problem as it was a pretty old one which could not handle the compression format.
    After deleting this unzip I was able to install CCS5.2 without problems ......

    I'm still wondering why the installer relies on a local unzip. On another PC there is no unzip in the PATH but
    installation worked pretty well .....

    Best regards,
    Mario 

  • Hi Mario,

    glad to hear it is sorted.  All the best with things.

    Best Regards,
    Lisa