This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello,
I am using CC4 with purchased license and also free license. both work fine.
What is the difference between free and paid version? is the paid version better? and in what way?
thank you,
Vishwanatha
Hi
We People Mostly Used Free Version. But I Personally Recommended to all that we should always use Licence Version. In the Licence Version if any Problem occure so easily recovered and do not lost your data as well. free software sometimes works well but when it crashed it's lost all the data.
Thanks
Hi,
I could not understand completely what data is lost. Could you explain a bit more?
thank you,
Vishwanatha
Hello,
the answer to your question in part depends on the hardware you use. Basically the answer for CCv4 is
MSP430/C2000 - the difference between the free and full version is that the free version is code size limited.
For other hardware that contains a free version - these versions are hardware dependent. For example use of the XDS100 emulator is free with CCS. There is no limiation on these licenses aside from the hardware allowed to connect.
Hope this clarifies and helps.
Best Regards,
LIsa